DENVER, Oct. 17, 2019 /PRNewswire/ -- Gates (NYSE: GTES), a leading global provider of application-specific fluid power and power transmission solutions, announces the latest innovation in smart crimper technology. The GC20™ with Gates® Cortex™ Intelligence takes the guesswork out of hose assembly fabrication and features intuitive touch-screen controls, on-board training, integrated eCrimp™ settings and remote support. The patent-pending GC20 Cortex is a smart and versatile solution for ultimate operational efficiency in both the factory and the field.
"The GC20 with Gates Cortex Intelligence represents the continuation of the digital revolution at Gates," said Mike Haen, vice president, global product line management. "Our digital strategy is to develop and launch IoT solutions that provide tangible benefit for the next generation of customers and align with Industry 4.0. The GC20 Cortex is connected in a way that makes our customers' jobs easier and improves their ability to consistently make high quality hydraulic assemblies in the field."
The GC20 Cortex is a purposeful upgrade to the well-known Gates Power Crimp® 707 (PC707) crimper and, while it retains all of the former crimper's capabilities, this product features new technological advances designed to further safeguard crimper operations, including upgrades that solve common pain points and exceed user expectations. Additional features of the GC20 Cortex include:
"Gates has tens of thousands of PC707 crimpers actively in use across North America," said Haen. "A retrofit kit is available to upgrade existing PC707 crimpers to GC20 Cortex crimpers with a straightforward 45-minute conversion. The GC20 Cortex uses the same pumps and dies as the PC707 crimper, so customers can benefit from this innovation with minimal disruption or extra expense."
See the GC20 Cortex live at AAPEX, November 5-7, 2019. To schedule an interview on-site, contact Ani Vattano, or visit booth #4038.
Gates will launch the GC20 with Gates Cortex Intelligence in the U.S. and Canada in Q4 2019, and is currently accepting pre-orders. For more information, visit www.gates.com/gc20.
About Gates
Gates is a global manufacturer of innovative, highly-engineered power transmission and fluid power solutions. Gates offers a broad portfolio of products to diverse replacement channel customers and to original equipment ("first-fit") manufacturers as specified components. Gates participates in many sectors of the industrial and consumer markets. Gates products play essential roles in a diverse range of applications across a wide variety of end markets ranging from harsh and hazardous industries such as agriculture, construction, manufacturing and energy, to everyday consumer applications such as printers, power washers, automatic doors and vacuum cleaners, and virtually every form of transportation. Gates products are sold in 128 countries across four commercial regions: the Americas; Europe, Middle East and Africa; Greater China; and East Asia and India. More about Gates can be found at www.gates.com.
SOURCE Gates
Actualités
June, 15, 2021 — Gates (NYSE: GTES) has accepted an invitation to become a member of the Advisory Strategies Planning Group at the National Fluid Power Centre (NFPC).The representatives of member companies work closely with NFPC engineers to develop a clearer understanding of their product ranges, how to install and use them, as well as how to maintain them to increase overall levels of performance.
EN SAVOIR PLUS
Gates lance la NOUVELLE courroie synchrone GT4™ avec un webinaire en direct
oct. 2020 — Gates hydrauliques et mécaniques, lance la courroie PowerGrip™ GT4™, une nouvelle courroie synchrone à couple élevé en élastomère d'éthylène (EE) par le biais d'un webinaire en direct.
EN SAVOIR PLUS
sept. 2020 — Gates hydrauliques et mécaniques, vous aide à faire la différence entre les revêtements de tuyaux hydrauliques « enveloppés » ou « lisses ». Cindy Cookson, directrice de la gamme de produits hydrauliques Gates, vous présente un aperçu des propriétés spécifiques de chacun des revêtements et essaie de déterminer si l'un est « meilleur » que l'autre.
EN SAVOIR PLUS