DENVER, March 20, 2019 /PRNewswire/ -- Gates (NYSE: GTES), a leading global provider of application-specific fluid power and power transmission solutions, has further expanded its PRO™ Series portfolio with the launch of a new ProXT™ hydraulic hose line and an all-new line of PRO Series couplings.
The Gates PRO Series line of professional-grade hydraulic hoses and couplings offers performance specifically tailored to hydraulic applications across multiple end markets. Leveraging Gates' deep application knowledge, materials science expertise and process engineering capabilities, the full line of PRO Series products delivers performance, reliability and design flexibility to meet the varying demands seen in today's hydraulic systems.
With the addition of the new ProXT hoses, the Gates Pro Series line is now global and meets the vast majority of global industry hose specifications demanded by replacement and first-fit customers. The new ProXT hoses will be available in seven sizes ranging from ¼ to 1 inch and meet SAE 100R2/R16, ISO 11237 R16 and EN 857 2SC industry performance standards. Gates is also actively developing a PRO Series Pro1T hose to address the EN 857 1SC industry standard.
Gates PRO Series couplings are qualified for use with the full line of PRO Series hoses, including ProXT, to ensure end-to-end system performance. The matched PRO Series coupling line covers all popular terminations with corresponding crimp specifications published online. Gates technical experts and engineers are available to evaluate and optimize customers' system designs to ensure the right solution for each application.
"By continuing to expand our PRO Series line of hoses and couplings, our customers now have a broader portfolio for selecting the right product for their application," said Tom Pitstick, CMO and senior vice president of Product Line Management for Gates. "Complementing Gates' existing line of MegaSys® hose and couplings, the PRO Series line allows us to grow with our existing customers across channels and meet the needs of new customers by providing a broader range of engineering solutions for modern hydraulic applications."
ProXT and the PRO Series coupling line are being introduced in North America, with a rollout planned across additional regions later in 2019.
About Gates
Gates is a global manufacturer of innovative, highly engineered power transmission and fluid power solutions. Gates offers a broad portfolio of products to diverse replacement channel customers and to original equipment ("first-fit") manufacturers as specified components. Gates participates in many sectors of the industrial and consumer markets. Gates products play essential roles in a diverse range of applications across a wide variety of end markets ranging from harsh and hazardous industries such as agriculture, construction, manufacturing and energy, to everyday consumer applications such as printers, power washers, automatic doors and vacuum cleaners, and virtually every form of transportation. Gates products are sold in 128 countries across four commercial regions: the Americas; Europe, Middle East and Africa; Greater China; and East Asia and India. More about Gates can be found at www.gates.com.
Forward-Looking Statements
This press release contains forward-looking statements. All forward-looking statements involve risks and uncertainties which could affect our actual results and could cause its actual results to differ materially from those expressed or implied in any forward-looking statements made by, or on behalf of, us. Important factors could affect our results and could cause results to differ materially from those expressed in our forward-looking statements, including but not limited to the factors discussed in the section entitled "Risk Factors" in Gates' Annual Report on Form 10-K for the fiscal year ended December 30, 2017, as filed with the Securities and Exchange Commission.
SOURCE Gates
Actualités
June, 15, 2021 — Gates (NYSE: GTES) has accepted an invitation to become a member of the Advisory Strategies Planning Group at the National Fluid Power Centre (NFPC).The representatives of member companies work closely with NFPC engineers to develop a clearer understanding of their product ranges, how to install and use them, as well as how to maintain them to increase overall levels of performance.
EN SAVOIR PLUS
Gates lance la NOUVELLE courroie synchrone GT4™ avec un webinaire en direct
oct. 2020 — Gates hydrauliques et mécaniques, lance la courroie PowerGrip™ GT4™, une nouvelle courroie synchrone à couple élevé en élastomère d'éthylène (EE) par le biais d'un webinaire en direct.
EN SAVOIR PLUS
sept. 2020 — Gates hydrauliques et mécaniques, vous aide à faire la différence entre les revêtements de tuyaux hydrauliques « enveloppés » ou « lisses ». Cindy Cookson, directrice de la gamme de produits hydrauliques Gates, vous présente un aperçu des propriétés spécifiques de chacun des revêtements et essaie de déterminer si l'un est « meilleur » que l'autre.
EN SAVOIR PLUS