Products
  • Products
  • Content

    Gates Introduces 3" and 4" Data Master™ MegaFlex™ Hoses to Unlock Higher-Capacity Cooling for Data Centers

    New large‑diameter hoses open access to more applications—supporting higher flow rates and improving installation efficiency across cooling loops 

     

    DENVER, May 11, 2026 -- Gates Corporation (NYSE: GTES), a global manufacturer of innovative, highly engineered power transmission and fluid power solutions, is expanding its Data Master MegaFlex hose portfolio with new 3-inch and 4-inch inner diameter options. The larger sizes are purpose‑built for the increased cooling capacity and higher flow rates demanded by next‑generation AI, hyperscale and HPC facilities.

     

    Data center cooling systems are being pushed harder than ever as rack power densities begin to reach 150-plus kW per rack, coolant flow requirements are dramatically increasing. The expanded Data Master MegaFlex line delivers the flexibility, durability and flow capacity required for large‑diameter data center cooling applications. The new 3-inch and 4-inch ID hoses give designers and operators greater freedom to build scalable systems that meet liquid cooling requirements.

     

    “The cooling demands and the subsequent flow requirements are rapidly increasing,” said Rebekah Headley, general manager of the Gates data center business unit. “By adding 3‑inch and 4‑inch diameters to the Data Master MegaFlex line, we’re giving a broadened set of solutions to address equipment and on-site coolant conveyance.”

     

    What the Expansion Delivers

    • OCP aligned: large-bore 3-inch and 4-inch ID hoses align with OCP liquid cooling guidance by enabling high-flow, low-pressure-drop performance in primary and CDU loops, while supporting material compatibility and flexible routing. 

    • Enables new applications: optimized for technology‑cooling system source lines and Coolant Distribution Units (CDUs).

    • Reduces system contamination: proprietary zinc‑free peroxide-cured EPDM tube materials protect coolant purity and critical components.

    • More efficient installation: up to 75% tighter minimum bend radius (MBR) versus competing hoses reduces kinking and rework, while eliminating cleaning, passivation and welded connections required for rigid steel piping.

    • Increases cooling capacity: larger IDs support greater coolant flow across data center cooling loops.

    • Reduces system pressure drop: reduced hydraulic resistance, lowering pump head requirements and improving cooling loop efficiency.

    Real‑World Deployment Validates Performance

    In a recent multi-building data center expansion, engineers faced tight routing spaces, aggressive construction schedules and the need for large-ID lines to support high-flow liquid cooling. They selected Data Master MegaFlex, which combines specialized zinc-free peroxide-cured EPDM tube material for coolant compatibility and fast, kink-free installation, enabling the higher flow needed for cooling loop distribution and CDU integration. Gates' local distribution network supplied custom cut-to-length assemblies, helping the contractor stay on schedule across multiple build phases. The result: higher capacity cooling through larger flow paths, maximizing usability, flexibility and coolant cleanliness. The project demonstrated how larger diameter Data Master MegaFlex hoses can accelerate construction timelines while delivering the higher flow rates required for modern cooling architectures.

     

    The expanded Data Master MegaFlex hose line and the full Gates Data Center Solutions portfolio are available globally. For specifications or to speak with a cooling systems expert, visit gates.com/datacentersolutions.

     

    About Gates Industrial Corporation 
    Gates is a global manufacturer of innovative, highly engineered power transmission and fluid power solutions. Gates offers a broad portfolio of products to diverse replacement channel customers and to OEMs as specified components. Gates participates in many sectors of the industrial and consumer markets. Our products play essential roles in a diverse range of applications across a wide variety of end markets, ranging from harsh and hazardous industries to everyday consumer applications, including virtually every form of transportation. Our products are sold in more than 130 countries across our three commercial regions: the Americas; Europe, Middle East and Africa; and Asia-Pacific. For more information, visit  gates.com.

    Latest Insights

    • Data Master™ MegaFlex™ Expansion

      DENVER, May 11, 2026 - Gates Corporation (NYSE: GTES), a global manufacturer of innovative, highly engineered power transmission and fluid power solutions, is expanding its Data Master MegaFlex hose portfolio with new 3-inch and 4-inch inner diameter options. The larger sizes are purpose‑built for the increased cooling capacity and higher flow rates demanded by next‑generation AI, hyperscale, and HPC facilities.

      Data Master™ MegaFlex™ Expansion
    • CFMOTO Race Team Sponsorship

      March 11, 2026 - Gates Corporation (NYSE: GTES), a global manufacturer of innovative, highly engineered power transmission and fluid power solutions, today announced its official sponsorship of the CFMOTO ASPAR Moto2 Team competing in the Moto2 World Championship. The collaboration aligns two innovation-driven companies committed to advancing performance, engineering precision, and global brand growth within the motorcycle industry.
      CFMOTO Race Team Sponsorship
    • SEAL Award Winner 2026

      Mar. 13, 2026 - Gates Corporation (NYSE: GTES), a global manufacturer of innovative, highly engineered power transmission and fluid power solutions, announced it has received a 2026 SEAL Sustainable Product Award for Data Master™ Eco. The award recognizes the product’s contribution to more sustainable, high-performance operations in mission-critical data center environments.
      SEAL Award Winner 2026