DENVER, Dec. 3, 2019 /PRNewswire/ -- Gates (NYSE: GTES), a leading global provider of application-specific fluid power and power transmission solutions, introduces a new line of continuously variable transmission (CVT) belts specifically designed to withstand the increased heat, power and operating environments of today's off-road vehicles (ORVs).
Gates G-Force™ RedLine™ CVT belts are engineered from a patented, fiber-reinforced Ethylene Elastomer compound, providing maximum transverse stiffness and unmatched heat resistance which allows for increased durability, greater load-carrying capability and a higher effective operating temperature. Extensively lab and field-tested, ATV and UTV enthusiasts and racers alike can expect break-through performance as Gates G-Force RedLine belts deliver:
"Today's high-performance ORVs demand innovative belt technology than can withstand use in the most extreme environments," says Christian Buhlmann, vice president of global product line management for Gates. "Through advanced materials science and process technology, we've created the next generation of CVT power transmission belts designed to deliver higher load capacity, higher peak torque capacity, less heat fatigue and greater durability."
In addition to the performance benefits, Ethylene Elastomers are more environmentally friendly to manufacture and will serve as the foundation for future belt developments at Gates across a number of categories.
Gates G-Force RedLine belts are now available from select powersports distributors across North America. To learn more, and to see the G-Force RedLine in action, please visit www.gates.com/redline.
About Gates
Gates is a global manufacturer of innovative, highly engineered power transmission and fluid power solutions. Gates offers a broad portfolio of products to diverse replacement channel customers and to original equipment ("first-fit") manufacturers as specified components. Gates participates in many sectors of the industrial and consumer markets. Gates products play essential roles in a diverse range of applications across a wide variety of end markets ranging from harsh and hazardous industries such as agriculture, construction, manufacturing and energy, to everyday consumer applications such as printers, power washers, automatic doors and vacuum cleaners, and virtually every form of transportation. Gates products are sold in 128 countries across four commercial regions: the Americas; Europe, Middle East and Africa; Greater China; and East Asia and India. More about Gates can be found at www.gates.com.
SOURCE Gates Corporation
Actualités
June, 15, 2021 — Gates (NYSE: GTES) has accepted an invitation to become a member of the Advisory Strategies Planning Group at the National Fluid Power Centre (NFPC).The representatives of member companies work closely with NFPC engineers to develop a clearer understanding of their product ranges, how to install and use them, as well as how to maintain them to increase overall levels of performance.
EN SAVOIR PLUS
Gates lance la NOUVELLE courroie synchrone GT4™ avec un webinaire en direct
oct. 2020 — Gates hydrauliques et mécaniques, lance la courroie PowerGrip™ GT4™, une nouvelle courroie synchrone à couple élevé en élastomère d'éthylène (EE) par le biais d'un webinaire en direct.
EN SAVOIR PLUS
sept. 2020 — Gates hydrauliques et mécaniques, vous aide à faire la différence entre les revêtements de tuyaux hydrauliques « enveloppés » ou « lisses ». Cindy Cookson, directrice de la gamme de produits hydrauliques Gates, vous présente un aperçu des propriétés spécifiques de chacun des revêtements et essaie de déterminer si l'un est « meilleur » que l'autre.
EN SAVOIR PLUS