DENVER, Feb. 19, 2019 /PRNewswire/ -- Gates (NYSE: GTES), a leading global provider of application-specific fluid power and power transmission solutions, introduces the PowerGrip® GT®4 belt, a newly designed ethylene elastomer (EE) high-torque synchronous belt for industrial markets.
The PowerGrip GT4 reflects Gates' dedication to innovation in materials science and process engineering. Many of the elastomer synchronous belts in the market today are made using chloroprene, a material that has performance limitations. The new Gates PowerGrip GT4 belt construction replaces chloroprene with a special EE formulation that delivers much higher performance. The company pioneered ethylene elastomer technology with its line of Micro-V® belts in automotive markets and applied that materials science technology to PowerGrip GT4 for industrial markets.
PowerGrip GT4 has the highest power-carrying capacity in the segment, a larger temperature range and improved chemical resistance. This allows for narrower drives and a broader range of applications to be served. For machine builders, this creates design flexibility and improves the ability to fit a belt drive into smaller spaces or to utilize more torque. Distributors can differentiate with a higher-performance offering and end-users running industrial drives as part of their operations experience a lower total cost of ownership. The improved performance characteristics also support additional market opportunities with the conversion of roller chain to belt drive solutions, enabling a transformation from a high-maintenance chain to a high-performance belt.
"PowerGrip GT4 extends the success we've had with the PowerGrip family of industrial belts over many years by upping the performance bar," said Tom Pitstick, CMO and senior vice president of Product Line Management for Gates. "It's right at home in heavy-duty industrial environments driving pumps, conveyor systems and other machinery where efficiency, reliability and high quality are required. PowerGrip GT4 belts eliminate the need for lubrication and maintenance, run quietly and reduce contamination risks, further extending our ability to replace traditional chain drives in key end markets."
Gates will offer a full portfolio of PowerGrip GT4 belts in 8mm and 14mm tooth pitches, and lengths exceeding 6.5 meters. Samples are available now with full-scale production beginning in North America and Europe in Q2 2019, with Asia to follow later in the year.
About Gates
Gates is a global manufacturer of innovative, highly engineered power transmission and fluid power solutions. Gates offers a broad portfolio of products to diverse replacement channel customers and to original equipment ("first-fit") manufacturers as specified components. Gates participates in many sectors of the industrial and consumer markets. Gates products play essential roles in a diverse range of applications across a wide variety of end markets ranging from harsh and hazardous industries such as agriculture, construction, manufacturing and energy, to everyday consumer applications such as printers, power washers, automatic doors and vacuum cleaners, and virtually every form of transportation. Gates products are sold in 128 countries across four commercial regions: the Americas; Europe, Middle East and Africa; Greater China; and East Asia and India. More about Gates can be found at www.gates.com.
Forward-Looking Statements
This press release contains forward-looking statements. All forward-looking statements involve risks and uncertainties which could affect our actual results and could cause its actual results to differ materially from those expressed or implied in any forward-looking statements made by, or on behalf of, us. Important factors could affect our results and could cause results to differ materially from those expressed in our forward-looking statements, including but not limited to the factors discussed in the section entitled "Risk Factors" in Gates' Annual Report on Form 10-K for the fiscal year ended December 30, 2017, as filed with the Securities and Exchange Commission.
SOURCE Gates
Actualités
June, 15, 2021 — Gates (NYSE: GTES) has accepted an invitation to become a member of the Advisory Strategies Planning Group at the National Fluid Power Centre (NFPC).The representatives of member companies work closely with NFPC engineers to develop a clearer understanding of their product ranges, how to install and use them, as well as how to maintain them to increase overall levels of performance.
EN SAVOIR PLUS
Gates lance la NOUVELLE courroie synchrone GT4™ avec un webinaire en direct
oct. 2020 — Gates hydrauliques et mécaniques, lance la courroie PowerGrip™ GT4™, une nouvelle courroie synchrone à couple élevé en élastomère d'éthylène (EE) par le biais d'un webinaire en direct.
EN SAVOIR PLUS
sept. 2020 — Gates hydrauliques et mécaniques, vous aide à faire la différence entre les revêtements de tuyaux hydrauliques « enveloppés » ou « lisses ». Cindy Cookson, directrice de la gamme de produits hydrauliques Gates, vous présente un aperçu des propriétés spécifiques de chacun des revêtements et essaie de déterminer si l'un est « meilleur » que l'autre.
EN SAVOIR PLUS