Sprocket Coating Extends Belt Drive Life on Triumph Motorcycles
Triumph motorcycles are known the world over for classy design and creative engineering. Those qualities extend to their latest model introduction, the Thunderbird, and its belt drive system.
Based in Hinckley, England, Triumph Motorcycles has a long history of engineering innovation. In 2004, Triumph began developing a mid-size cruiser. The market places certain demands on cruisers. They need a clean-running final drive, and long intervals between maintenance to keep them on the road. Both these demands call for a belt drive system. But Triumph hadn’t manufactured a belt-driven motorcycle since the 1920s.
According to Simon Warburton, Triumph’s Product Manager, “Belt drives were new to us, so we needed a partner who knew what they were doing. We recognized Gates preeminence in this field.”
Gates engineers took on the challenge. They knew the limitations of conventional belt drives, whose die-cast or billet aluminum sprockets typically lasted only 2,000 – 5,000 miles. Gates is no newcomer to motorcycle belt drives. Earlier drive designs with Gates Poly Chain® GT® belts running on hard chrome finished sprockets were lasting 30,000 – 50,000 miles. Belt and sprockets wore at about the same rate, so manufacturers advised users to replace both at the same interval.
But then along came Gates Poly Chain® GT® Carbon® belt. With stronger-than-steel carbon tensile cords, this belt was outlasting the sprockets. Worn sprockets shredded the belt prematurely. So Gates and Triumph turned to the sprockets to develop a more durable, corrosion-resistant coating that would yield a longer-running drive system.
Essentially, the goal was to make the sprockets last as long as the belt. Gates engineers took a hard look at today’s industrial hard chrome metal finishes. They explored adding more coating material. They experimented with new formulations. But one hurdle kept presenting itself: hexavalent chromium.
The traditional hard chrome plating process produces hexavalent chromium waste, a human carcinogen (remember Erin Brockovich?). The EPA is lowering threshold limits on hexavalent chromium, resulting in new and costlier plating and waste disposal techniques. So Gates and Triumph went looking for a “greener” coating—one that would provide even greater durability and corrosion resistance than hard chrome plate.
Gates engineers tested dozens of coatings. The best contenders were sent to Triumph for salt spray resistance testing and live tests on motorcycles. The winner was called Gates Armour-GK™. This proprietary coating produces a surface that outperforms hard chrome plate by a factor of 5 to 1 in terms of wear resistance . The coating’s chemistry and method of application to the base metal form a nearly impregnable “skin.” And it’s environmentally friendly in the bargain.
Now the Thunderbirds are rolling off the assembly line. The bike was unveiled in Barcelona, Spain, in May 2009. Sixty-five journalists rode, prodded and penned with enthusiasm. And the question was frequently asked: “Is it a Gates carbon belt drive?” The answer: “Yes, and Gates Armour-GK sprockets as well.” Time will tell, but tests indicate that this belt drive could go twice the miles of competitor cruisers before belt or sprockets need to be changed.
You can check out Triumph’s Thunderbird at http://www.triumph.co.uk/USA/
What can Gates do for you? For help with your application, speak with a Gates product application engineer at 303-744-5800, or email ptpasupport@gates.com.