Gates Complete Spiral Launch
To meet the needs of a burgeoning industry, Gates launched its Complete Spiral Solutions at a mega-event in Mumbai, India. With the growth in economy, sale of high end and capital intensive Construction Equipment is on the rise. Considerable growth is being demonstrated in the Heavy Earthmoving and Mining Machinery segment and is a derivative of increased focus and investments vis-a-vis Infrastructure and Construction sectors. Although Hydraulic Hoses in particular and Fluid Conveyance in general find myriads of applications across the industrial canvass, but the spiral hose finds significant consumption by construction equipment segment.

Setting high standards in technology and R&D, and in order to meet the vast demands of the industry, Gates Complete Spiral Hoses & Couplings were launched in the presence of key customers and OEMs at the Taj Mahal Palace Hotel, Mumbai, on 19th Jan, 2011. The importance of the event is evident from the fact that to support this endeavour Mr David Gau, President, Global Fluid Power Division, Gates Corporation, USA took out his time and graced the occasion. He was accompanied by Mr Nitin Kaul, Director Tomkins. and Mr. Jaideep Wadhwa, President, Tomkins (I&A) India.

Gates Spiral Hoses were available earlier as well but complete solution package was missing, With the inclusion of GS (Global Spiral) Couplings, a complete solution offering is now available, Crimped to Gates Specs – ensuring the benefits of highly advanced Gates Interface Technology being available to the market. These advanced products offer many Features, Advantages and Benefits for the customers. Gates Complete Spiral Hoses & Couplings exceed the SAE Specs and meet the most stringent Quality Standard expectations of global OEMs.

Gates Spiral Hoses offer Flexibility, Durability and Reliability of a remarkably high degree.
• Flexibility – Contrary to the competitors' products which are rigid and un-flexible, Gates system performs at Half SAE Bend Radius.
• In terms of Durability, the spec for spiral hoses is 500,000 impulse cycles, whereas Gates hoses are tested to perform more than 1 Million Impulse Cycles.
• Reliability comes through Gates design which ensures trouble-free long life.
• The recommended Hose with recommended couplings ensure all the above parameters when crimped to Gates Specifications.

Such intricate interface technology and associated crimp data are all available with Gates Authorised Assemblers. Practice of mix-n-match ends up in huge losses of money and downtime. Hence insistence on Authorised Assembler certification is advised by Gates in order to get best value for money.

At the launch event, technical presentations and USPs of the products were highlighted by different speakers and audience asked pertinent questions. Gates India also showcased its strengths through two Audio Visual films made especially for the occasion. A special inaugural scheme was announced to motivate the customers to experience the benefits of Gates System in Extreme High Pressure applications. Gates also took feedback from the august gathering on how to further improve its products and services.

A Distributor Meet was scheduled for the next day pre lunch session, ie. 20th Jan., 2011 – a gathering of Gates Distributors who are the major promoters of Gates Spiral Hoses and System across the country. This also included an Awards presentation where high-performers & achievers from amongst the Channel Network were honored by Mr David Gau, while Mr Bhandari announced the special scheme for distributors and also thanked all guests for sparing their valuable time. Once again team games and fun activities kept the visitors engrossed and after lunch at the Taj, everybody was taken over to a cruise for the evening where light entertainment, song and dance awaited them in all frolic.