Expo's

EXCON 2011


Gates participated at Excon 2011, the 6th International Construction Equipment And Construction Technology Trade Fair from 23-27 November,2011 at Bangalore International Exhibition Centre, Bengaluru and was organized by Confederation of Indian industries. Excon 2011 with its new ideas / trends has in the store the best opportunity for Companies to network and further strengthen the existing business and establish newer ones. Excon 2011 will be the ideal platform for not only the Indian companies but also for the International buyers & Investors. Gates has been a part of Excon from 2007 and this has been its third participation in the biannual Trade fair.








IMX 2011,Pune

The 2011 Industrial Maintenance Expo (IMX) was held in Pune from 4 November 2011- 6 November 2011 at the Auto Cluster Exhibition Centre, Pune. This 3 day exhibition was organized by the Confederation of Indian Industry & it mainly featured on service, maintenance & care. Some of the important highlights of this exhibition are face to face meeting with buyers, explaining condition monitoring and focus on B2B Market.



Process Engineering Expo 2011


INDIAMART PROCESS ENGINEERING EXPO 2011 was the first of its kind in India, held in Hyderabad from September 1-3, 2011, organized by M/s Synergy Exposures & Events India Pvt Ltd., Chennai and M/s Hyderabad International Trade Expositions Ltd. (HITEX), Hyderabad. This focused mainly on the large and varied Process Engineering sector which is spread widely across the length and breadth of the country.

The objective of participating in the Process Engineering Expo 2011 was to provide a meeting platform to both end-users and dealers and to showcase the range of Gates products especially the soon-to-be-launched Megasys Hose. This enabled us to reach the majority of the users of our products and services in a very short period and in a well-planned manner, thereby showcasing our product innovations. The novelty of this exposition is that it is not restricted to any particular product segment or any individual user of the industry, but with a focus on the multifaceted process related industries. The focused industry segment for this expo will include Cement, Chemical, Steel, Power, Metallurgy, Fertilizer, Paper, etc., all of which have the application of hoses to generate end products.



IFEX 2011


Gates participated in IFEX 2011 – the 7th International Exhibition on Foundry Technology, Equipment and Supplies (organized by
IIF -- THE INSTITUTE OF INDIAN FOUNDRYMEN) held at Chandigarh, India between 11th to 13th Feb., 2011. The specially crafted Gates India stall was well appreciated and visitors thronged for a glimpse of various Gates products customized for the Foundry and Metal Industry

The Chief Guest Mr. Jagat Shah, Managing Director, Inductotherm India, who was kind enough to take out time and grace the occasion inagurated the Gates stall and also launched GAJRA – the new premium Coke Injection Hose from Gates. Gajra is recommended for highly abrasive particles like coke particles, Gravel, Sand or a mixture of all with air. Especially recommended for extreme abrasive conditions where normal Sand Blast Hoses are not able to perform. It outperforms any hose in such severe working conditions. A special Feature is that extra thick tube is added for a superior abrasion resistance and is suitable for lasting for a minimum of 70 heats in steel melting conditions. The USPs of Gajra Hose are:

High Abrasion Resistance
Superior Technology for Longer Life
Available in Exact Lengths
Proven at Steel Plants

Continuing with the goal of Total Solution Provider, for the Foundry Industry – Gates offers Carbon Free hoses for Furnace Coolant Applications alongwith World-Class Stainless Steel Hose Clamps. As a part of System Selling Approach, Gates is now entered into annual rate contracts with major players like Inductotherm and Electrotherm for Gates Clamps in addition to Carbon Free Hoses. Gates commands almost 90% market share in this segment.

The USPs of Gates Carbon Free Hoses – With excellent low leakage current less than 20 Micro Amp. At 6000V D.C., it is recommended for Furnace Coolant and Electrical Cable Coolant Applications in Steel Industry and other Non-Conductive Applications. Experts at Gates developed this special product with the innovation of new rubber based compounds required to meet the demanding performance requirements in Furnace Coolant Applications. Gates Carbon Free Hose is a highly efficient product which offers features like low leakage current (less than 20 micro Ampo at 6 KV DC) and significantly longer life.

Gates Ideal SS Clamps are Rust Free high-tensile Clamps ideally suited for Furnace Applications which result in lower number of clamp consumption. Features & Benefits of Gates Ideal Clamps are:

Ultra-strong Gripping Power
Enhanced Corrosion Resistance
One-piece Interlocked Housing
Rectangular Slotting of Bands
More Coverage Area
Better Inventory Management
Large Hose Range Capability
Economical

Concurrent to the IFEX, the 59th Indian Foundry Congress was also organized by the IIF at Chandigarh. Gates participated in this premier congregation as part of the Tech Mart Seminar on 12th Feb by presenting a paper on advancements in solutions for the Foundry Industry. Overall, Gates India had a successful event where its offering and presentation was appreciated by one and all.



PETROTECH 2010

GATES ANNOUNCES QUICK RESPONSE CENTER at PETROTECH,2010
Gates Corporation are pleased to announce the establishment of our 37th Quick Response Center in India. Gates Quick Response Centers are dedicated oil, gas and marine service outlets offering the complete range of Gates Oilfield products and services.

Gates Engineering & Services is globally headquartered in Dubai, United Arab Emirates and is 100% owned by the Gates Corporation of Denver, Colorado whom have over 100 year of manufacturing and development experience.

Gates Engineering & Services in India will be a seamless operation within the global Engineering & Services business unit and will be supporting all of our major global clients as they expand into the important Indian market.

Gates Engineering & Services are the world's leaders in fluid engineering and will be expanding the range of infield services such as hose management via reliability services technicians.

Gates India is offered a Tata Nano Car to the lucky winner visiting their stall at the Petrotech expo. Utilizing the Petrotech-2010 platform the company launched its new look Website with complete product range www.gates.com/india

We also launched our next year's Calendar on the theme of "We value our heritage" which is in line with our centennial celebration.

A number of new product launches were also undertaken during the exhibition which includes the range of Dry Disconnect Couplings and Valves.

For further details please visit www.gates.com/oilfield or contact at customercare@gatesind.com


Auto Expo 2010

Gates made its presence felt at the AutoExpo head it Pragati Maidan, New Delhi in Jan'10. The Gates renage of Automotive Products were showcased. A very good response was received as this was our maiden presence in this domain.












Engg. Expo, INDORE

We participated with our Indore Distributor M/s TIRUPATI TECHNOCHEM in Engineering Expo in Madhya Pradesh. Overwhelming response was received for Gates Products & Services. Customers were delighted by the wide range of product range & the reach of the Gates Channel Partners in this territory of Central India.

Machinery Mart, 09-12 March 2010, GUWAHATI

An Expo organized by CII North East wing to create a buyer seller platform for Engineering products required by Customers of North East. There is a major Infrastructure development work Going on in this part of the country which slightly lagging behind as compared to the rest of the Country.

Gates India have put up a Stall showcasing their Hydraulics product range of Hoses ,Couplings, Adapters, QRCs Clamps etc for creating a Brand awareness in this part of the Country. We have got good response from this show as a lot of positive leads are generated from this Brand awareness activity & our team of Local Marketing Representatives are working on the same to convert into prospects.