Gates Corporation   Gates Corporation
The world's most trusted name in belts, hose and hydraulics.
 
search
Gates USA/Canada
Worldwide
industrial section automotive section
Content Tools
Feedback Feedback Form
Print Format Print Format


Timing Belts

  Part Store Locator 

Timing Belt Replacement - GatesGates is the only manufacturer approved by virtually every major OEM to provide timing belts for new engines.

This means that Gates is able to cover the aftermarket with timing belts that are OE-equivalent or better in service life and performance.

Gates also has the largest selection of timing component kits for the aftermarket, with 75 percent of its kits being specified for import vehicles.  Each kit for 1974 - 2004 model years contains all the parts needed for a timing belt system replacement: one or more timing belts, idlers and/or tensioners, and detailed instructions. 


Timing Belt Replacement GuideCatalog PDF - Gates

Timing belt replacement intervals for all major autmobile makes and models.

When the automaker doesn't make a specific recommendation, Gates suggests changing the timing belt at 60,000 miles.

Timing Belt Replacement Cover

 

 
 

Exact Fit for Imports

 

Gates has the largest coverage for import engine applications ranging from Acura to Yugo vehicles.

  OE-Match timing belts 
  Timing Belt


 

Interference Engine Issues

Got an Interference Engine?
Find Out Now  

Timing belt-equipped car engines can be classified as either free-running or interference, depending on what occurs if piston/valve synchronization is lost due to a failed timing belt. As illustrated below, an interference engine usually sustains damage if synchronization is lost. This could result in very expensive engine repairs.

Interference1


No Valve/Piston Interference

Interference2


Valve/Piston Interference

Notes: Timing belt failure on interference engines can result in serious engine damage. See manufacturer's maintenance manual for specific information. Belts of similar dimensions and tooth profiles are not interchangeable due to varying construction features. Misapplication of belts voids manufacturer's warranty. 


 

 Auto Data Ad

Need Specs?
espec. de la necesidad 


 
  Additional Timing Belt Info
 

 Product Application Engineers

Automotive Catalog Collection

 Part Locator & Interchange

Timing System Tools

 Timing Belts Limited Warranty Catalog PDF - Gates


Replace a Belt or an Engine?  Service Reminder Logo


Timing Component Kits - Belt, Idler and Tensioner pulley

In the aftermarket, "job comebacks" are one of the biggest concerns for installers. They greatly reduce productivity and profitability, not to mention the loss of repeat business and negative word of mouth.

In the case of the timing belt system, Gates Rubber Company engineers have determined that belt failure "comebacks" are often caused by a faulty timing belt idler or tensioner pulley.

Gates line of Timing Component Kits allow you to service the complete timing system - including the belt(s), idler(s), tensioner pulley(s) and installation instructions.

Part Store Locator 

Ad Timing Kit

 

 

Timing Component KitsCatalog PDF - Gates

 Each kit contains:   Belts
   Idlers
   Tensioner pulleys
   Installation instructions

More than 120 timing component kits available.
    Most extensive coverage in the industry.
    Tough, wear-resistant fabric on working surfaces.
    Special materials resist oil and engine heat.
    High tensile strength cord construction minimizes stretch.
    Approved for marine applications. 

Note: Order Timing Component Kits and Oil Seals at the same time for less frustration.

Oil Seals - Ensure Maximum Timing Belt Life

To help installers do a complete job of replacing the timing belt drive system, Gates has a line of cam and crankshaft oil seals.

The seals will prevent oil contamination to a newly installed timing belt assembly, ensure maximum belt life and reduce costly "comebacks" that may result from future leaks at the cam and crankshaft.

Gates engineers recommend that installers replace these oil seals whenever they install Timing Component Kits to ensure the best replacement service and maximum customer satisfaction.

Oil Seals Info & list of Applications Catalog PDF - Gates

 

Part Store Locator 

TCK+Seals

More than two-dozen oil seal kits for domestic and import cars are available from Gates. Each kit contains one, two or three seals, depending on the application. 


Water Pumps

Gates is the most preferred and trusted supplier of cooling system belts and hoses.

Gates now offers you a line of new – not remanufactured – water pumps, designed and built for long lasting, efficient cooling. 

Water Pumps 

Part Store Locator 

Water Pump Box

 


 
E-Z Download
What kind of file is this? Timing Belt Replacement Guide 884 KB (4 minutes
at 28.8 kbps)
What kind of file is this? Timing Belts Limited Warranty 13 KB (4 seconds
at 28.8 kbps)