Gates Corporation   Gates Corporation
The world's most trusted name in belts, hose and hydraulics.
 
search
Gates USA/Canada
Worldwide
industrial section automotive section


Now that you have looked at our product info, are you now looking to purchase Gates products?
Yes, I know what I want.
No, I still need more information from Gates.com.
No, I need to speak with at least one person.
No, we are just looking for information right now.


Checked your belts lately?
The most recent Car Care Council survey found that 24% of belts checked were in need of replacement.

Content Tools
Feedback Feedback Form
Print Format Print Format


Troubleshooting V-ribbed Belt Noise
 

Terms such as chirp, squeal, rumble and yelp have been used in the automotive industry to describe noises caused by friction-induced vibration in engine accessory drive belts. The following report, based on testing by Gates Corporation, examines primary causes and remedies for this problem.

 

To the educated ear, drive belt noise can be as
distinctive as the notes on a musical scale.
 

 
Additional V-ribbed  Belt Info
   Product Application

   Automotive Catalog Collection

   Part Locator & Interchange

 

 

Under-The-Hood Harmonics

    All sounds that are audible to the human ear have their origins in some vibrating surface. For example, intermittent chirping that increases in frequency as the engine is revved up can be the result of belt vibration caused by misaligned drive pulleys -- a leading cause of belt noise. As a misaligned V-ribbed belt span enters the grooves of a pulley, initial contact is made with only one side of the V-groove. The greater the misalignment angle, the greater the radial sliding length experienced by the belt ribs as the belt seats in the pulley causing frictional vibrations, or chirping (see Figure 1).

    Figure 1  

    Radial sliding motion of V-ribbed belt. 

    Low belt tension, contamination and belt vibration are other common sources of belt noise. A screeching or squealing noise that occurs when pulling away from a stop normally indicates a lack of tension; check belt tension and automatic tensioners

    A tapping or grinding noise caused by a pebble imbedded in the belt is a common occurrence. Grinding sound also can result from damaged bearings, which must be replaced, aligned and lubricated to eliminate the noise and further damage. 

    Vibration and noise can develop over time as drive components such as pulleys and spring tensioners wear out of tolerance, as bearings and brackets loosen, or as belts wear and stretch.

Diagnosing The Problem

In ongoing studies at the Gates Belt Testing Laboratory in Denver, engineers have gained the following insights to noise resulting from misalignment: 

  1. Chirp noise caused by drive misalignment occurs upon entry of the span into the pulley as belt ribs seat into the pulley grooves, not as the belt exits.                   
  2. Belts are less likely to generate misalignment noise when they are in new condition. As belts wear in, they develop a smooth, glossy surface which increases the likelihood for noise. This wear-in process is accelerated when misalignment conditions exist in the drive.                   
  3. The angle between belt span and pulley is the critical factor responsible for causing the "chirp" associated with misalignment noise. Misalignment angle can result from many different combinations of pulley positions -- parallel and angular are two ty pical examples (see Figures 2 & 3).

    Figure 2  

    Parallel misalignment. 

    Figure 3  

    Angular misalignment. 

     

  4. Misalignment noise occurs most frequently on the shortest spans in a drive, most often between a backside pulley and an adjacent accessory pulley. Proper pulley alignment is particularly critical in these locations.                   
  5. Flat or crowned pulleys have no grooves to guide the belt and can be a common source of drive misalignment.                   
  6. Smaller diameter pulleys exhibit less sensitivity to misalignment noise due to their smaller area of sliding contact between the belt and pulley.                   
  7. Misalignment noise is generally loudest at idle speed and diminishes with increasing engine rpm, often vanishing altogether above 2500 rpm.                   
  8. The presence of high humidity (or a damp belt) often increases the likelihood for misalignment noise to occur.

In The Shop

Whenever a vehicle owner complains of belt noise, Gates says it is important to determine the type of noise and under what circumstances it occurs. A solution to a noise problem caused by drive misalignment is not likely to resolve a slip noise problem th at may be caused by insufficient tension or some other problem. Find out if the problem is more noticeable in the morning while the engine is cool (cool, damp belt). Is the noise loudest at idle speed, or when accelerating or shifting gears (rapid changes in engine speed can cause a belt to slip)?

Next, attempt to recreate the problem in the service bay. Using a spray bottle filled with water, mist the belt lightly. If the noise level recedes for several seconds, then returns louder, a misalignment problem is likely. If the noise immediately increa ses after the belt is sprayed, slipping is likely. 

If the water spray test is inconclusive, or not successful at diagnosing the problem, attempt to remove the noisy belt and re-install it so that the belt runs in the opposite direction. Because misalignment noise is influenced by the direction of misalign ment in the drive, flipping the belt around in this manner will eliminate or significantly diminish (temporarily) any noise caused by drive misalignment. If the noise remains unchanged, the problem is not likely related to drive alignment. 

In actual applications, the highest occurrence of belt noise due to misalignment comes from short belt spans entering large diameter pulleys. Service technicians are encouraged to look for the source of noise wherever these conditions exist. 

Also, look for replaced drive components, such as a rebuilt alternator, which may have been improperly installed resulting in pulley misalignment.

Corrective Action

Failure to correct conditions responsible for belt noise will result in the problem returning, usually within 3,000 miles or less.

If the problem is drive-related, depending on the degree of misalignment, it may be possible to modify the noise level by installing a new belt with noise-resistant properties. 

Gates engineers have developed new elastomeric compounds that are noise-resistant under various environmental and wear conditions. These new belts feature additives that enable them to slide easily into and out of the pulley. This low-noise construction h elps to eliminate belt noise from most misalignment situations. 

In the case of severe misalignment, repositioning of drive components using shims, or by changing the press fit of the pulley or the shaft, may be required. Pulley alignment and tension must be correct on all V-ribbed belt applications for the drive to operate properly.