Gates Carbon Drive Launches Lower Priced Belt Drive for City Bikes

Mar 11, 2015

Same carbon technology, designed for relaxed city and urban riding

DENVER – Gates Corporation, maker of the chain-replacing belt drive system for bicycles, is launching a “value oriented” product line designed for lower-mileage pavement and city bikes.

The Gates Carbon Drive CDN™ system has the same carbon fiber tensile cord technology and CenterTrack sprocket design as Gates’ premium CDX™ system, but at about half the cost.

“CDN is our value-oriented belt drive for people who want a clean and stylish city bike for getting into town or around the neighborhood,” says Todd Sellden, director of Gates Carbon Drive. “It’s for bicyclists who ride in jeans or skirts and casual shoes, not spandex and race gear.”

The CDN belt has nine carbon cords embedded within an engineered polymer belt with a patented 11 millimeter tooth pitch profile optimized for lower tension. The front sprocket is made from reinforced composite embedded with glass fibers and comes as an integrated crank assembly for easy factory installation. The rear sprocket is wear-resistant steel.

Five years in development, the CDN belts are manufactured at the Gates plant in Dumfries, Scotland, a leading producer of automotive belts and the center for Gates’ belt development group in Europe. CDX and CDC™ belts are still manufactured in the USA at the Gates plant in Kentucky. CDX remains the application for mountain biking, cyclocross racing and long-distance bike touring.

Gates will launch CDN at the Taipei Bike Show and is currently booking appointments. “Interest is high,” says Frank Scurlock, global sales director for Gates Carbon Drive. “Brands have been asking for this, with the goal of using it on high volume bike models for the general public.”

Hi resolution images of CDN can be downloaded at

About Gates Carbon Drive 
Consisting of two lightweight sprockets and a high-strength belt embedded with carbon fiber cords, Gates Carbon Drive™ is a low-maintenance, chain-replacing technology from Gates Corporation, the global leader in automotive and industrial belts. Clean, quiet, light, and strong, Carbon Drive requires no greasy lube, weighs less than a chain drive and will not stretch. Due to its low maintenance and ease of use, Carbon Drive is a technology that can get more people on bikes. Gates Carbon Drive is featured on more than 200 bike models from more than 100 brands in 2015. Find your bike at

Register to Access Your Resource